MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [Closed] Low frequency response of IIS3DWB

I have been characterizing the sub 200Hz characteristic of the IIS3DWB, and we are aware that it is somewhat an uncharted territory.But I was somewhat surprised by my observation when I compared a piezoelectric sensor attached to an IIS3DWB, vibrated...

0693W00000GWdQ1QAL.png 0693W00000GWdPwQAL.png
MAnil.1 by Associate II
  • 4000 Views
  • 4 replies
  • 0 kudos

Resolved! LPS22HB I2C communication error due to pin3 ?

Hello,We are developing a STEM-based educational product. We have just received our initial test PCB for V2.In our PCB for sensing the pressure, we have used an LPS22HB pressure sensor, I am attaching the circuit diagram used for the LP22HB in the PC...

0693W00000GVy7rQAD.png 0693W00000GVy7wQAD.png 0693W00000GVy8VQAT.png 0693W00000GVy8fQAD.png
DBhav.1 by Associate II
  • 2264 Views
  • 2 replies
  • 0 kudos

Tap detection in low power for LIS2DS12

LIS2DS12 has Tap detection functionality. The ODR (output data rate) has to be >=400 Hz is stated in the datasheet. In low power mode ODR of 400 Hz en 800 Hz are supported (10 bit) resolution. Is Tap detection supported in low power mode? I cannot f...

Lama by Associate III
  • 1590 Views
  • 2 replies
  • 0 kudos

Resolved! Values for lm6dsox acc values in non movement state?

HelloIm using steval mksbox 1vs1 for vibration analysis. I have taken measurements with motor in movement and withe the motor stopped. At first I supose that with the motor in stop mode, the acc values in the 3 axis should be near to 0. In other thre...

NMart.1 by Associate III
  • 1115 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.