Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
In I2C mode for the IIS3DWB device the datasheet says it only support single axis mode because I2C is too slow to get the data. I want to use I2C mode to configure either wake up or activity thresholds for all 3 axis and then configure the interrupt...
Hi,I'm using ULD to get measurements from VL53L1X. My case need to get 9 ROI - divided FoV into 3x3. When I run such measurement procedure it with 2x2 = 4 RoI - It's okay. But when I get 3x3 RoI in a similar way I get measurements such as max u16_t =...
We are using the FIFO compression feature of the LSM6DSO32 which is working well for us if we use it standalone at 833 Hz. When we add the 4 FSM's that handle our motion recognition we start seeing duplicate tags in the compressed output implying tha...
I have been looking for Linux drivers for the LSM6DS33 "iNEMO inertial module:always-on 3D accelerometer and 3D gyroscope", but have not had any luck. If anyone knows about any such repos or even references, it would be greatly appreciated.Thanks!
サンプルアプリをIAR�?�カスタマイズ�?��?�使�?��?��?��?��?�。アプリ�?�android�?�サンプルアプリを使�?��?��?��?��?�。注�?点�?��?�を教�?��?��??�?��?��?�。
here is my circuit for the LSM9DS1i used the code from sparkfun breakout moduel to test the board. i can get the data from their board, but not my board.
In my project, I used the LIS3DH chip. Most of the time the processor sleeps.The processor wakes up on time and on exceeding the shock threshold.In case of awakening on shock threshold, I need to read the data from the FIFO buffer (32 measurements) t...
Hello,I'm using a LIS2DTW12, here the configuration :ODR 400HzFIFO threshold on INT2 push pull interrupt. Threshold 16Continuous mode All seems to work correctly but sometimes I have an incorrect interrupt. The INT2 signal is yellow, the purple is a ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.