cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSL FIFO data misalignment (XYZ rotated) and FIFO_PATTERN always 0 — how to align reads?

Manoj_Bidari
Associate

Case Description:



Title: LSM6DSL FIFO data misalignment (XYZ rotated) and FIFO_PATTERN always 0 — how to align reads?

Body:

I’m using an LSM6DSL over I²C with an STM32. Goal: batch accelerometer-only samples into FIFO and drain clean (x,y,z) triplets at a fixed watermark. I keep running into two issues:

  1. Data misalignment — the XYZ triplets appear “rotated”. I’ll get a few normal lines, then a line where one column looks like a big random number (e.g., ~168xx), then it stabilizes again. Example:
x,y,z
5, 250, 16870,
17, 258, 16825,
-66, 221, 16828,
-53, 284, 16834,
Sampling End
Sampling Start
-22, 4, 242,
16846, 13, 281
16830, 51, 230
16882, 39, 242
16850, 11, 258
16803, -14, 220
16843, -24, 232
16855, 0, 241
  1. FIFO_PATTERN is always 0 — I expected to use FIFO_STATUS3/4 (FIFO_PATTERN[9:0]) to know which axis comes next and align before parsing, but I always read 0, even when the FIFO is clearly non-empty and STOP_ON_FTH has fired.

Hardware

  • LSM6DSL @ 3.3V, I²C 400 kHz
  • SDO tied low → 7-bit addr 0x6A
  • MCU: STM32 (HAL I²C)

Config summary (accelerometer-only)

  • CTRL1_XL: ODR = 833 Hz, FS = ±2g, high-perf
  • CTRL2_G: 0 (gyro off)
  • CTRL3_C: BDU=1, IF_INC=1, BLE=0 (little-endian)
  • FIFO_CTRL1/2: watermark = 1536 words (for 512samples × 3 words/sample)
  • FIFO_CTRL3: BDR_XL = NO_DEC, BDR_GY = DISABLE
  • FIFO_CTRL4: STOP_ON_FTH = 1, ONLY_HIGH_DATA = 0
  • FIFO_CTRL5: ODR_FIFO = 833Hz, FIFO_MODE = STREAM
  • TIMER_PEDO_FIFO_EN=0FIFO_TEMP_EN=0 (don’t want timestamp or temp in FIFO)

Sanity checks:

  • WHOAMI is correct, soft reset works.
  • DIFF_FIFO reports levels that match watermark (in words).
  • Endianness is little; parsing uses int16_t from LSB/MSB correctly.
  • Reading from FIFO_DATA_OUT_L with auto-increment.

What I tried

  • Reading FIFO_PATTERN (STATUS3/4) right before burst read. It always returns 0, so pattern % 3 == 0 and my code assumes next word is X, but the log suggests I’m sometimes starting at Y or Z.
  • Toggling STOP_ON_FTH on/off and changing ODRs.
  • Ensuring temp/timestamp/DS3/DS4 are disabled so only accel data is batched.
  • Full device reset between runs.
1 ACCEPTED SOLUTION

Accepted Solutions
Saket_Om
ST Employee

Hello @Manoj_Bidari 

Did you try with the BSP LSM6DSL Component driver? 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

View solution in original post

3 REPLIES 3
Saket_Om
ST Employee

Hello @Manoj_Bidari 

Did you try with the BSP LSM6DSL Component driver? 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

Hello Saket,

Yes, i am using the BSP_LSM6DSL Component driver, even though i am facing the problems.

We would appreciate your guidance on resolving these issues.

Hello, any update regarding this issue? i am having similar problems.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.