MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C communication failure while reading data from VL53l0x

Hello,I am currently working with STM32wl55jc. My application invlolves few I2C sensors.The application also invlolves VL53l0x. These sensors have been mounted on a single PCB.I have tried explaining the problem below.1. I am currently reading the se...

Snatu by Associate II
  • 4849 Views
  • 7 replies
  • 0 kudos

Resolved! Are the three axes of LIS3MDL orthogonal?

As far as I know, the LIS3MDL is an excellent 3-axis tmr sensor. What I want to know is whether the magnetic field components of the XYZ axes measured by the LIS3MDL sensor are strictly orthogonal, and do I need to do some calibration before using it...

Resolved! MP34DT05-A PDM: increase SAI clock frequency

Hello everyone,I have an application that eventually record some audios and is working fine with a pair of MP34DT01. It works over SAI with a clock of 1.024MHz and a decimation factor of 64 (for the PDM2PCM), leading to an audio frequency of 16kHz.Th...

TVare.1 by Associate III
  • 2389 Views
  • 2 replies
  • 0 kudos

LIS2DH12TR- Not working on 3.3V.

Hello,I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greate...

Smalik by Associate II
  • 1334 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.