MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH12TR- Not working on 2.9V and above voltages

Hello,I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greate...

Smalik by Associate II
  • 1525 Views
  • 1 replies
  • 0 kudos

Resolved! How to activate auto-increment for lps25hb?

I'm using a nucleo f401re with a lps25hb. Currently I'm getting very wrong values, this is caused by the reading of the registers. For example when I call the registers of temperature which is composed by two bytes HAL_I2C_Mem_Read(&hi2c1, LPS25HB_I2...

YGail.2 by Associate III
  • 2244 Views
  • 3 replies
  • 0 kudos

MotionFX Flash and RAM Size Problem

I would like to use the MotionFX Library from the X-CUBE-MEMS1 package in a project on a STM32WL55JC.The datasheet of the library states the following:Cortex-M4: 44.1 kB of code and 1.1 kB of data memoryI have already written a library for another ap...

JonasQ by Associate
  • 1343 Views
  • 1 replies
  • 0 kudos

Why doesn't the use of rounding for FIFO reading work for the lmsdso32 the way it did for the lmsd6DSL. The app notes describe exactly the same process for both?

We have been using rounding successfully for 3 years to access data from the FIFO of an lmsd6DSL to a connected micro computer via the SPI bus. The lmsdso32 app notes describe exactly the same process for rouding reading of the fifo which we are usin...

MByrn.2 by Associate
  • 1113 Views
  • 0 replies
  • 1 kudos

How to due with the gyro original data?

Dear ST engineers:​ I'm using a 6 axis IMU module (lsm6dsltr) for my project and this picture is the gyro original data. My parameters of the module is LSM6DSL_2000dps with 260mHz filtering chain. The figure shows a vibration circumstance that a...

0693W00000Y7F6EQAV.jpg
Zbobo.1 by Associate III
  • 1464 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.