MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSOX: FIFO buffer not full when interrupt received.

Hey guys, I use a LSM6DSOX chip to collect data from both accelerometer and gyroscope. I used the integrated FIFO feature, with the following configurations:Accelerometer/gyroscope batch ODR = 104HzFIFO mode is Continuous modeInterrupt on INT2 is rou...

0693W00000Y9IyXQAV.png
MZhan.8 by Associate
  • 1293 Views
  • 0 replies
  • 0 kudos

Resolved! Need 8000 degrees-per-second

I have successfully designed a product which uses ISM330DHCX. However this unit only allows for a maximum of +/- 4000 dps, and within the application of the product, the gyro can saturate at high speeds.Are there any plans on releasing a product that...

Nate by Associate
  • 2762 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.