cancel
Showing results for 
Search instead for 
Did you mean: 

Can Somebody extract a functional project using MXCUBE with usb_audi_in form Microphones_streaming (X-CUBE-MEMSMIC1)?

tcg
Associate III

Hi, I spend a lot of days trying to undestanding Microphones_streaming from X-CUBE-MEMSMIC1. That is very complex example and brillant at the same time. I want to extract the part for usb audio in streaming (device to pc), but it is a little crazy. it is important for me obtain a basic project for sending a randowm buffer. Then I want to create a support pack for ioc. Was some one able to generate a functional project only with this part? I ak for help to support but i can not be able to make with these indications. Thanks for your time

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
SimonePradolini
ST Employee

Hi @Tomás Cabeza​ ,

I'm not sure I got your point: do you need an example that sends random data instead of microphone ones?

If so, you can just simply pass your "random buffer" to the Send_Audio_to_USB function called into AudioProcess.

Something like this:

void AudioProcess(void)
{
  if (CCA02M2_AUDIO_IN_PDMToPCM(CCA02M2_AUDIO_INSTANCE, (uint16_t *)PDM_Buffer, PCM_Buffer) != BSP_ERROR_NONE)
  {
    Error_Handler();
  }
Send_Audio_to_USB((int16_t *)your_random_buffer, (AUDIO_IN_SAMPLING_FREQUENCY / 1000)*AUDIO_IN_CHANNELS * N_MS);
}

X-CUBE-MEMSMIC1 is not supported in CubeMX.

The microphone sampling frequency directly depends from the clock tree. Those values are strictly defined into the BSP_AUDIO file.

As for now, CubeMX is not able to read BSP files and import a bounded clock tree.

That's why we can't distribute MEMSMIC1 as a pack and there is no .ioc available.

I wish my answer can help you.

Feel free to further comment to find a proper solution for your use case.

Best regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.