MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to slove the problem which the register's storage space of the ASM330LHHX is smaller than external sensor 's connected?

I connected the ASM330LHHX(STM sensor featuring a 3-axis digital accelerometer and a 3-axis digital gyroscope) and INA228(one of the TI sensors measuring the current and voltage) via the I2C interface. What's more, I want to read the data from the AS...

SWu.6 by Associate
  • 1052 Views
  • 1 replies
  • 0 kudos

Interfacing PDM digital microphones using STM32 MCUs and MPUs

Hi,At Application Note 5027: "Interfacing PDM digital microphones using STM32 MCUs and MPUs" it described how to connect PDM microphone to SPI I/F of STM32. My question is:at SPI I/F clock is active only when there is SPI transaction, how can I caus...

AShpi.2 by Associate
  • 2119 Views
  • 1 replies
  • 0 kudos

Resolved! Detecting a short isolated event using lsm6dso32x

Hi,I'm trying to use LSM6DSO32X to detect a short (<5ms) event isolated by at least 100ms from other events (before and after). It's on the Y axis and with a threshold of 500mg. I'm not having any luck setting up a single TAP event or by using FSM. A...

IRogo.1 by Associate II
  • 1383 Views
  • 1 replies
  • 1 kudos

AIS3624DQ returning same vale on all three axis

Hi,I configured the AIS3624DQTR sensor by using standard driver given by ST on GitHub, I am able to set all parameter correctly but when I am trying to read X,Y and Z axis. It is returning same value on all axis and value is not changing by moving se...

Myada.2 by Associate
  • 1428 Views
  • 1 replies
  • 0 kudos

Content of LPS22DF i3c IBI payload?

I have an LPS22DF sensor connected via I3C. I can enable I3C in-band-interrupts (IBIs), and see the IBIs occur on data-ready events.I see the IBIs have a 5-byte data payload, but I can't find any definition of the data in this payload. Is this descri...

RoHS Exemptions 7(a) & 7(c)-I Remove Plan

Refer to the RoHS pack 22 Final report, RoHS exemptions 7(a) and 7(c)-I are possible to be expired on July 1, 2024. Could you please advise if STMicroelectronics has any plan to remove exemptions for the below parts? LD1117DT33TRSM15T100CASTPS8H100G-...

YYao.1 by Associate
  • 1918 Views
  • 1 replies
  • 0 kudos

Resolved! How does the LIS2DH accelerometer generate its clock, and what could be causing the sampling frequency discrepancy in its interrupts?

I'm working with the LIS2DH accelerometer and I'm trying to obtain acceleration data at a rate of 100 Hz. However, I've noticed that the accelerometer interrupts have a frequency of 99 Hz. Also this frequency changes if I use another accelerometer of...

ADelb.1 by Associate
  • 2723 Views
  • 3 replies
  • 1 kudos

STEVAL-MKI208V1K conecting to nucleo F401

Hello I want to connect to the STEVAL-MKI208V1K via STEVAL-MKIGIBV2 (conected those both togheter) , with Nucleo-F401RE. I conected pins as it is shown belowF401RE-> MKIGIBV2MOSI (PB3 -> SDAMISO -> SDOSCK -> SCLPWM/D6 -> CS3v3 -> VDDGND- >GNDI want t...

KDług.1 by Associate
  • 1808 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.