MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MotionFX correct sequence

Hi everybody and thanks in advance for the support.I have a ST SensorTile and I'm starting with the DataLog project to output data through USB port. I have correctly integrated MotionFX libraries and they seem to run, except there are just a bit of p...

peppea82 by Associate II
  • 2771 Views
  • 2 replies
  • 0 kudos

Accelerometer lsm6dso and ism330dlc not working

I am working on a project which has 2 board revisions A and B.(A was the old revision and B is new). Board A has the accelerometer chip lsm6dso and board B has the accelerometer chip ism330dlc. The driver used is drivers/iio/imu/st_lsm6dsx/. If I use...

smoha.2 by Associate II
  • 1230 Views
  • 1 replies
  • 0 kudos

PDM to PCM via DFSDM getting nothing but static

On the BL47E-IOT01A2 there are two mems microphones (MP34DT01) both connected to DFSDM1_DATIN2. I'm trying to extract the data from just one of those boards and convert it to PCM using a DFSDM filter. I've configured DFSDM Channel 2 to connect to PDM...

RBair.3 by Associate II
  • 1990 Views
  • 1 replies
  • 0 kudos

LSM6DSL Drift Specifications

Hello, ST engineers. I am working with a general purpose IMU for a tilt sensor application. I am observing some drift on the sensor while the device is off. I have heard that all IMU's can drift a bit, but I was under the impression that it would hap...

RBurg.2 by Associate II
  • 5451 Views
  • 5 replies
  • 0 kudos

LIS2DH registers saved before Power Off

Hello. I am using a LIS2DH board (STEVAL-MKI135V1). I use the STEVAL-MKI109V3 board and the UNICO-GUI app to configure the LIS2DH board. I configure it for Wake-Up system for X axis. So, I change the register for only enable the axis x and it works o...

javier by Associate
  • 871 Views
  • 1 replies
  • 0 kudos

Why I can´t connect the SensorTile.box to cloud ?

Facing some problems with the ST BLE Sensor App. Whenever I try to connect the device to cloud (Azure) it shows connection error ( in both android and IOS Phones).The SensorTile.Box I´m using is STEVAL – STLCR01V1

IBen .2 by Associate
  • 1052 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.