2023-02-09 11:29 PM
Hello I want to connect to the STEVAL-MKI208V1K via STEVAL-MKIGIBV2 (conected those both togheter) , with Nucleo-F401RE. I conected pins as it is shown below
F401RE-> MKIGIBV2
MOSI (PB3 -> SDA
MISO -> SDO
SCK -> SCL
PWM/D6 -> CS
3v3 -> VDD
GND- >GND
I want to use SPI 4 wire interface but immediately after connecting nucleo to the PC I lost conection to the board and led LD1 starts blinking red. Do I need to connect some other pins as well with a board? Do I need to use some pull up resistors to the pins?
2023-04-12 6:57 AM
Hi @Konrad Długozima ,
You need to connect also VDDIO to 3V3.
Let me know if this solve your problem and in case please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.