MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FFT feature extraction on Unico

Hello, I recently started working with Unico GUI software and I need to do a classification task for soundwaves with already gathered data using the decision tree from the MLC but I would like the classification based on features that can be extracte...

SRodr.4 by Associate II
  • 1534 Views
  • 1 replies
  • 0 kudos

MotionMC calibration process.

Hello everyone. I make some project based on MotionMC and MotionEC libs. It's a magnetic compass which will use inside the cars. Within the MotionMC library, the end device functions properly if calibrated according to section 2.2.5 of the UM2192 man...

ALT.1 by Associate
  • 1309 Views
  • 0 replies
  • 0 kudos

LIS2DTW12 SENSOR IC

Dear Sir/Madam,​I am trying to configure x axis, y axis and z axis in LIS2DTW12 SENSOR IC interfacing with NUCLEO-L476RG microcontroller when board is towards sky direction. These are the values in z axis1.26 in (+-2g configuration), 2.046 in (+-4g c...

ggowd.1 by Associate III
  • 5261 Views
  • 13 replies
  • 0 kudos

Resolved! Is it possible to use the ULTRA LITE DRIVER (SWST-IMG009) for VL53L1X to manage and control the VL53L1 ToF Sensor?

Hi! My name is Vincenzo.Taking a look at the two sensors, I started to believe that they are similar in terms of Architecture, more precisely it seems to me that the VL53L1 has expanded the characteristics of the VL53L1X at the expense of a slightly ...

VNava by Associate III
  • 4459 Views
  • 6 replies
  • 1 kudos

Resolved! LIS2DW12 Current Consumption.

Hello STMicroelectronics Support Team, I am currently working on a development project where I'm utilizing the LIS2DW12 accelerometer. However, I've encountered an issue with the current consumption of the accelerometer on our custom board. I wo...

VMali.2 by Associate
  • 2967 Views
  • 3 replies
  • 0 kudos

LSM6DSR FSM and Activity/Inactivity Triggers

Is there a way to move between inactive sample rate and regular sample rate with FSMs enabled?I have configurations written from the host microcontroller to the LSM6DSR in which I can enable or disable double tap and enable or disable the FSM(s) in t...

_legacyfs_online_stmicro_images_0693W00000dJwLpQAK.png

Resolved! What is the LSM6DSL life cycle?

ST(Semiconductor) chip LSM6DSLTR, the website has NOT checked NRND(NOT RECOMMENDED FOR NEW DESIGNS) notice information, how long is the remaining life cycle of this chip?When is the expected date FOR the manufacturer to notify NRND(NOT RECOMMENDED FO...

xwang.6 by Associate III
  • 2550 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.