MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DW12 FIFO overflows upon wake-up by interrupt

GreetingsI have configured  the LIS2DW12, via SPI,  to sample and store samples, given the FIFO (configured in continuous mode) on a wakeup interrupt to INT1. The sensor, given its current configuration is able to wake up and sample but there is a wo...

ZAIDS-S23 by Associate III
  • 2730 Views
  • 4 replies
  • 0 kudos

Resolved! ST tile box pro heading drift issue

Hi all,I am using ST tile box pro and logging IMU orientation data for my test. I did place that module in a robotic arm and then calibrate the accel sensor. I observed 20 degree drift in the  heading value  after the calibration .Before calibration ...

Accelerometer and gyroscope

Hello,I need to measure the tilt angles (along the x, y, z axis) of a flying device. What accelerometer can you recommend produced by STM? Will one accelerometer be enough? Or do you still need a gyroscope to complete the task?

ASM330LHB on STEVAL-MKI236A difficulty connecting via I2C

I am trying to connect the IMU sensor that is onboard the STEVAL_MKI236AA evaluation board. I am currently trying to connect that board to BeagleBone AI-64 or a basic Arduino via I2C and was able to detect an I2C device as 0x6A and 0x6B as the board ...

PXL_20240127_174704392.jpg

Resolved! Unicleo-GUI does not connect

Hello,    I am trying to test the compass of the IKS4A1 board with a Nucleo F446 board. I followed line by line the instructions provided in the "Getting started with the STMicroelectronics X-CUBE-MEMS1 software package for STM32CubeMX". My cube proj...

MRaff1_0-1706287076093.png
MRaff.1 by Associate III
  • 2912 Views
  • 3 replies
  • 1 kudos

LSM303AGR X-CUBE-MEMS1

Hello,    I have a custom board with a STM32F373 and a LSM303AGR MEMS device.I made a Cube-MX project in which I included the corresponding x-cube-mems1 software pack with an eCompass application.The project compiles and runs. I see from the firmware...

MRaff.1 by Associate III
  • 1861 Views
  • 2 replies
  • 0 kudos

ULP mode LSM6DS032 configuration procedure

Hi all,Been trying to use the ULP mode on LSM6DS032 with following steps.1. Setting XL to Power down mode by setting XL_ODR bits to 0b0000  of CTRL1_XL register.2. Set I3C_DISABLE to 1 of  register CTRL9_XL. // Not sure if this is necessary3. Power d...

bimalpaneru_0-1706512371883.png

LIS2DE12 not reaching current consumption said in datasheet

Hello,I'm evaluating the LIS2DE12 accelerometer by using the combination of STEVAL-MKI175V1 and STEVAL-MKI109V3 along a Power Profiler Kit II from Nordic Semiconductors for current measurement.Method of test:I removed the jumper that source VDD, brid...

sch0bert_5-1705418750414.png sch0bert_3-1705418520338.png sch0bert_6-1705419238154.png sch0bert_7-1705419302266.png
sch0bert by Associate III
  • 3496 Views
  • 4 replies
  • 0 kudos

ASM330lhh

Hi,I am working with ASM330lhh, connected to my linux device via i2c.in the sysfs i can see the device with the command  "ls -l /sys/bus/iio/devices/iio:device1/"  that return:total 0 -r--r--r-- 1 root root 4096 Mar 24 14:21 consumers -rw-r--r-- 1 ro...

Orenzv by Associate
  • 2775 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.