2024-01-24 8:50 AM
Hello,
I have a custom board with a STM32F373 and a LSM303AGR MEMS device.
I made a Cube-MX project in which I included the corresponding x-cube-mems1 software pack with an eCompass application.
The project compiles and runs. I see from the firmware it is waiting from commands from uart. So I run the unicleo-GUI and connect to the corresponding port but nothing happen. Is the unicleo-GUI sw intended to run only with the SDK? Is there some other sw I have to use?
Thank you.
2024-01-25 12:47 AM
I found that sending from the terminal this sequence:
\h(32)\h(01)\h(0C)\h(09)\h(1B)\h(2A)\h(18)\h( 01)\h(19)\h(04)\h(3D)\h(F0)\h(32)\h(01)\h(02)\h(CB)\h(F0)\h(0D)\h(0A)
the board replies.
The difference compared to Unicleo-GUI sent command seems to be the termination \h(0D)\h(0A).
2024-01-29 9:52 AM
Hello @MRaff.1,
It should work, maybe some configuration in the project is not correct. Can you share you .ioc file so I can check it?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.