MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! shock Survivability LPS27HHTW

Hi,  I want to know the shock survivability of the pressure sensor LPS27HHTW but I didn't find it in datasheet or application notes.Do you know an application note or data about its shock resistance Thanks for your help   

David45 by Associate II
  • 1401 Views
  • 1 replies
  • 1 kudos

Resolved! Top Marking information for LPS22HBTR

I couldn't find information about the topmaking for the nano sensor LPS22HB on the datasheet, I need to implement a visual inspection for this IC.Does anyone knows where I can find this info? 

LIS2DTW12 temperature sensor accuracy

Hello everyone,We manufactured about 100 boards for a pre-production run using the LIS2DTW12, and at room temperature, the boards are all over the map with +/-3°C accuracy, nowhere near the "typical" +/-0.8°C as stated in the datasheet.I've already s...

vard by Associate II
  • 4788 Views
  • 6 replies
  • 1 kudos

Resolved! Signal delay MEMS Studio BUG

I think signal delay library does not work on MEMS Studio.I made an example code to show temperature values from a nucleo-L476RG and x-nucleo-IKS01A3 setup.The code should show the actual value and a delayed one:But it gives the following error:This ...

aesteban_0-1715168691138.png aesteban_1-1715168772554.png
aesteban by Associate III
  • 1517 Views
  • 1 replies
  • 0 kudos

IMU long term stability

Hi,I encountered a problem with a couple of LSM6DSOX employed over 2 years in a mobile Hydraulcs application where the came back to factory for inspection and we saw a significant drift of the offset of the accelerometer (>200mg).Looking at the ASM33...

gioPic97 by Associate
  • 1978 Views
  • 1 replies
  • 0 kudos

Resolved! lis2dh12 returns constant data using STMems driver read data polling

I have several boards with lis2dh12 and all of them keeps return constant data for lis2dw12_acceleration_raw_get function, every board has its own constant, 0x5050, 0xe0e0, 0x7070.I tried using the STEVAL-MKI135V1 connected to STM3220G-EVAL to test m...

Ywo.1 by Associate II
  • 9441 Views
  • 17 replies
  • 0 kudos

Resolved! LIS2DW12's sensitivity setting

Hi,I am using LIS2DW12 to detect walking situation of old man.Old man is walking slowly and little moving, In order to detect this small moving, what and how do I set CTRL register you recommend?I have to check continuous moving state....If LIS2DW12 ...

Paul.Lee by Associate III
  • 4402 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.