2024-04-18 6:29 PM - edited 2024-04-18 7:02 PM
Hi,
I am using LIS2DW12 to detect walking situation of old man.
Old man is walking slowly and little moving,
In order to detect this small moving, what and how do I set CTRL register you recommend?
I have to check continuous moving state....
If LIS2DW12 is not suitable this acton, what do you recommend new chip?
BR
Paul
Solved! Go to Solution.
2024-05-09 12:45 AM
Hi, Federica,
TAP_THS_X/Y/Z threshold value were set little high value.
I have changed that value to 1, and become more sensitive and satisfied.
BR
Paul
2024-04-19 6:12 AM
Hi @Paul.Lee ,
If you want to use only the acceleration to detect walking, LIS2DW12 is fine.
I suggest you to set an high FS (16g for example) and low ODR, you could try 50Hz.
Hope this helps.
2024-04-20 9:41 PM
Hi,
+/-16g is more sensitive than +/-2g?
BR
Paul
2024-04-22 4:30 AM
I don't work for ST but I have used this accelerometer.
2g is much more sensitive. I suggest High performance mode, low pass filter with BW filter at maximum. LOW_NOISE enabled.
Fastest way I've found to test settings is using micropython using Thonny with a Rasperry pi pico. it's super simple and it has a built in live chart to see how your changes affect the readings.
2024-04-22 4:55 PM
Hi,
Thank you for help.
I have to be aware of battery power consumption, so I set to Low power mode.
I set 25Hz with low power mode 1. CTRL1 is set to 0x30
My device is using CR2032.
BR
Paul
2024-04-23 5:22 PM
Hi, Federica,
Please add a comment on this.
BR
Paul
2024-05-02 2:18 AM
Hi @Paul.Lee ,
I don't think you could have problems using low power instead of high performance. But I suggest you to increase the ODR to 50 Hz.
You can do a test with your settings and if you cannot discriminate steps change them.
2024-05-09 12:45 AM
Hi, Federica,
TAP_THS_X/Y/Z threshold value were set little high value.
I have changed that value to 1, and become more sensitive and satisfied.
BR
Paul
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.