MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power consumption of magnetometer lis2mdl

I used in the past lis2mdl. I need to reproduce the former product. I ordered the same parts but I faced an issue with the magnetometer. The part number is the same but i got different power consumption. I got an image with the different magnetometer...

IMG_20240502_153331.jpg
Kostas_N by Associate
  • 2175 Views
  • 3 replies
  • 0 kudos

Resolved! LSM6DSR Wake Up and Activity Detection

Hello, currently I am using LSM6DSR for developing my apps.I have tested this sensor for Wake Up detection with 218.75 mg threshold and Activity detection with 15.625 mg threshold without any issues.Is it possible to enable both of these detection at...

Unexpected behaviour with LSM6DSO32TR

Hi,We are using an LSM6DSOX IMU and Micron MT29F2G01ABBGDWB Nand Flash on a common SPI bus. We didn't see any issue until we upgraded the LSM6DSOX with an LSM6DSO32. The datasheet suggests that they are drop-in replaceable. Both the flash chip and IM...

UQure by Associate
  • 1706 Views
  • 1 replies
  • 0 kudos

LIS2DW12 - Condition for self-test failure

GreetingsI have been using the LIS2DW12 accelerometer for some time now, and have tried to set up the self-test functionality. Ironically, I've set it up according to the AN5038 app note pg.46 and it has never failed the self test. I am also analysin...

ZAIDS-S23 by Associate III
  • 1208 Views
  • 1 replies
  • 0 kudos

Use of IIS2MDC sensor

Hello.I am a graduate student who is conducting research using IIS2MDC and Arduino, a digital magnetic sensor of STMicroelectronics.I am currently using IIS2MDC and Arduino Uno to measure the magnetic fields in the form of sine waves generated from t...

fig2.jpg fig1.png 3.png
Jinlee by Associate
  • 2073 Views
  • 1 replies
  • 0 kudos

environment setup with lsm6dso16is sensor

Hi Team,I want to evaluate LSM6DSO16IS, I found one expansion board X-NUCLEO-IKS4A1 already mount this sensor and have corresponding software and projects accordingly, additionally in projects could use NUCLEO-F401RE board to communicate, but seems i...

ISM330DHCX sensor hub

Hey ,i have been trying to link ISM330DHCX sensor to external sensors.Problem :working with STEVAL-STWINKT1B board and the schematics for my sensor ISM330DHCX clearly cannot be configured to be connected to external sensors , even though it is allowe...

Resolved! ST IMU LSM6DSL- software or algorithm to implement in to our firmware to determine the speed/acceleration & distance from IMU data.

We are using ST IMU LSM6DSL in to our chipset/PCB.We are looking for ready to use software or algorithm to implement in to our firmware to determine the speed/acceleration & distance from IMU data.Is there any example code available for share?

IKhan.1 by Associate
  • 2899 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.