2024-05-08 4:16 AM
Greetings
I have been using the LIS2DW12 accelerometer for some time now, and have tried to set up the self-test functionality. Ironically, I've set it up according to the AN5038 app note pg.46 and it has never failed the self test. I am also analysing the averages obtained before and after the self test, and the calculated differences are always within the range specified in the datasheet. I believe I can expect it to fail if I move the sensor during the period I expect the self-test to be running. I've tried this to no avail, where the self-test will still pass.
The criteria and simulation for a failure is important as it will directly determine if my device using the IC, is ready to be used. Please may I be advised on any other methods to get the self-test to fail, or if it is plausible that I impose a tighter range on the min and max values that the calculated difference should fall in between.
Any help would be appreciated.
2024-05-23 2:51 AM
Hi @ZAIDS-S23 ,
The self test is to check the device functionality, the only way to see a failure is by breaking the piece.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.