2018-01-08 1:00 AM
hi,
i have a FATVolume.imf with 3 files. I use AT+S.FSUPDATE to download in wifi module.
Is it possible after it to delete 1 file with a cmd equivalent to AT+S.FSD (because this command has effect in the RAM memory volume and external SD card volume only and not User Flash) ?
Thanks
Yoann
Solved! Go to Solution.
2018-01-08 1:59 AM
Adding/removing files on a Flash disk is actually not supported. You can only erase it completely or download a new one.
Best Regards
2018-01-08 1:59 AM
Adding/removing files on a Flash disk is actually not supported. You can only erase it completely or download a new one.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.