Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPWF04Sx - delete file in User FS App Disk

Posted on January 08, 2018 at 10:00hi,i have a FATVolume.imf with 3 files. I use AT+S.FSUPDATE to download in wifi module.Is it possible after it to delete 1 file with a cmd equivalent to AT+S.FSD (because this command has effect in the RAM memory v...

LIN sensor problem

Posted on December 27, 2017 at 04:15I have a Pepper+Fuchs sensor which interface is LIN(attachements are datasheet & user manual ). I need to test the sensor by computer so I purchased RS232 to LIN converter. I send handshake command on computer to ...

0690X00000609IsQAI.png 0690X00000609IwQAI.png

BlueNRG BLE Throughput

Posted on December 13, 2016 at 12:50Hi,What is the maximum throughput one can achieve with either BlueNRG-MS or BlueNRG-1?I read that some BLE ICs has a chipset limitation on the number of packets transmitted in a single connection event (e.g., cann...

dudul by Associate
  • 5316 Views
  • 10 replies
  • 0 kudos

Security db problem

Posted on January 05, 2018 at 14:47Hi all,I am facing a problem with the security dababase, I am working with BLUENRG-1, I can paired two devices and getting them advertising and create connection, then close the connection and connect again...every...

jampino by Associate III
  • 592 Views
  • 0 replies
  • 0 kudos

SPWF04Sx - ip_use_dhcpd

Posted on January 04, 2018 at 11:02hi,SPWF04Sx + UART + FW1.1.0en.x-cube-wifi1_firmware_v3.1.0.zipwifi module is set in miniAP mode. i would like to activate dhcp server. Variable is 'ip_use_dhcpd' = 1 (on).But dhcp doesn't work!To set correctly the...

Connecting SPWF01SA to hidden SSID

Posted on September 05, 2017 at 10:47Hi,I need to have a SPWF01SA module connect to a Wi-Fi router with hidden SSID.The first operation the module tries upon starting is '+WIND:21:WiFi Scanning' which completes with the result '+WIND:35:WiFi Scan Co...

Luca DC by Associate II
  • 1987 Views
  • 5 replies
  • 0 kudos

[bug] Wrong sizeof in SimpleBlueNRG_HCI

Posted on December 07, 2017 at 15:43In the files STM32CubeExpansion_BLE1_V3.2.0\Middlewares\ST\STM32_BlueNRG\SimpleBlueNRG_HCI\hci\controller\bluenrg_hal_aci.cbluenrg_gap_aci.cWe can see some Osal_MemCpy with wrong sizeof. Ex in bluenrg_gap_aci.c:tB...

nicolas b by Associate III
  • 730 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.