2020-11-30 8:19 AM
Hello,
I'm working on the Nucleo-BNRG2A1 board.
Starting from the Virtual_COM_Port application in X-CUBE-BLE2 version 3.1.0, I have made modification to work on my L496ZG-P Nucleo Board.
When started the BlueNRG GUI 4.0.0, I have the following error popup:
"Old DTM fw detected. Update DTM fw."
On first test, version given by BlueNRG GUI were the following:
I used BlueNRG-W Flasher Utility with the DTM_SPI.hex file in BlueNRG GUI\Firmware directory to update the board. Now versions are the following:
But I still have the same error popup.
Is there anything else I can do to avoid this error?
In BlueNRG GUI I tryed the Stack Updater with no succes.
Thank you
Antoine
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.