Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STMIPID02 supports Selectable 0.81 or 0.9 D-PHY revision specification. Will you upgrade the chip to be compliant with MIPI D-PHY v2.5?

We purchased STMIPID02 couple of years ago and currently we want to support MIPI D-PHY v2.5 and MIPI CSI-2 v3.0. The STMIPID02 is too old and no similar chip updated in your solutions. Do you have any plan to deliver MIPI solution similar with STMIPI...

Sfu.2 by Associate
  • 720 Views
  • 0 replies
  • 0 kudos

BLE Chat application transfers are very slow

Hello,in our application, we are using STEVAL-STLKT01V1 boards.I ported the BLE Chat application from BlueNRG DK 2.0.2 to STEVAL-STLKT01V1 and I'm able to transfer data between client and server.However, I discovered that data transfer rate is quite ...

Problem with BlueNRG GUI and BNRG2A1 module

Hello,I'm working on the Nucleo-BNRG2A1 board.Starting from the Virtual_COM_Port application in X-CUBE-BLE2 version 3.1.0, I have made modification to work on my L496ZG-P Nucleo Board.When started the BlueNRG GUI 4.0.0, I have the following error pop...

ANauz.1 by Senior II
  • 808 Views
  • 0 replies
  • 0 kudos

Do we have any standard mobile app. from which we can transfer the chunk of data to ST BlueNRG2 chip?

I wanted to test one feature for my product where I need to transfer the chunks of data (in Hex) from mobile app to ST BlueNRG2 device.SO wanted to ask do we have such standard mobile app for free which can be used for testing the data transfer betwe...

BLUENRG change name "BlueNRG" doens't work

I have nucleo idb05a2 on board re401. i have compiled sensorDemo_BLEsensor-App. it work with Galaxy bluetooth 5.0 and not work with Honor bluetooh 4.2.Then i change name from "BlueNRG" to "TestBlue" (compiled and write) but still appired "blueNRG" st...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.