2026-01-20 5:10 AM
Hi ST Community,
I’m working with STM32WBA (STM32WPAN / BlueNRG-style stack APIs). I’m using Extended Advertising on the peripheral (connectable + scannable, secondary PHY = Coded) and a STM32WBA central that scans and then calls aci_gap_create_connection().
Problem
Connection is intermittent: sometimes it connects, but often the peripheral prints multiple times:
HCI_DISCONNECTION_COMPLETE_EVT_CODE - Connection Handle: 0x01 - Reason: 0x3E (repeats 4–5 times)
The central does retries very often, so the peripheral sees repeated disconnect events before it finally connects.
Setup details
Advertising set configured as connectable + scannable:
u16Property = HCI_ADV_EVENT_PROP_CONNECTABLE | HCI_ADV_EVENT_PROP_SCANNABLE;
Primary PHY = 1M, Secondary PHY = Coded (0x03):
aci_gap_adv_set_configuration(..., primaryPHY=0x00, secondaryPHY=0x03, ...)
Address type used in advertising set:
u8AddressType = GAP_STATIC_RANDOM_ADDR;
Advertising channels 37/38/39 enabled
TX power set via aci_hal_set_tx_power_level(1, CFG_TX_POWER)
Scan finds target via HCI_LE_EXTENDED_ADVERTISING_REPORT_SUBEVT_CODE
Central then calls aci_gap_create_connection()
Here is the current connect code (simplified):
result = aci_gap_create_connection(
SCAN_INT_MS(500), SCAN_WIN_MS(500),
GAP_STATIC_RANDOM_ADDR, // Peer_Address_Type <-- (my current code)
g_nSelection.pu8TargetAdr,
CFG_BD_ADDRESS_TYPE, // Own_Address_Type
CONN_INT_MS(7.5), CONN_INT_MS(7.5),
0,
u16ConnSupTimeout,
CONN_CE_LENGTH_MS(10), CONN_CE_LENGTH_MS(10)
);I also tried less aggressive intervals (e.g. Min 30 ms, Max 250 ms) and it got “better”, but the repeated 0x3E disconnect still happens sometimes.
Questions
For Extended Advertising connections, should the central use the peer address type from the advertising report (public/random) instead of constants like GAP_STATIC_RANDOM_ADDR?
My suspicion: I’m misusing Peer_Address_Type (should be 0=public / 1=random), and sometimes the stack interprets the peer address type incorrectly, leading to fast failure/disconnect reason 0x3E.
Is there a recommended stable set of parameters for:
LE_Scan_Interval / LE_Scan_Window during connection establishment
Conn_Interval_Min / Max for LE Coded / extended advertising
Minimum_CE_Length / Maximum_CE_Length (should these be 0?)
Any known issue/errata with STM32WBA + Extended Advertising + Coded PHY that can cause repeated disconnect reason 0x3E during initial connection?
Additional info
Peripheral prints repeated disconnect reason 0x3E before a successful connection happens.
Central is retrying connection frequently.
Addresses themselves look correct (I see the target address from scan and use it for connect).
Any guidance on correct use of aci_gap_create_connection() with Extended Advertising (especially peer address type handling) and recommended parameters would be greatly appreciated.
Thanks!
2026-03-09 2:44 AM
Hi,
From what you describe, the repeated 0x3E (Connection Failed to be Established) on the peripheral side is most often related to a noisy RF environment.
I also notice you are using aci_gap_create_connection() rather than aci_gap_ext_create_connection(). If this is not intentional ? it may be worth checking.
By the way, there are reference examples you can rely on if needed:
Peripheral: BLE_p2pServer_Ext
https://github.com/STMicroelectronics/STM32CubeWBA/tree/main/Projects/NUCLEO-WBA65RI/Applications/BLE/BLE_p2pServer_Ext
Central: BLE_p2pClient_Ext
https://github.com/STMicroelectronics/STM32CubeWBA/tree/main/Projects/NUCLEO-WBA65RI/Applications/BLE/BLE_p2pClient_Ext
BR, Joé
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.