2019-09-24 1:37 PM
Howdy, folks. I'm new to the ST universe but have plenty of embedded experience. I have a BlueNRG-2 evaluation board and an ST-Link interface that I have been working with. Here is the problem -
I can open a sample BLE peripheral example in Atollic TrueStudio, then successfully compile the application to Elf/Bin/Hex format. If I download that app using the UART loader for the board, it executes and runs normally. This is an unmodified sample program directly from ST.
If however I attach the ST-Link to the board and run the code from inside the debugger, it does not fully execute properly. The program loads, I get the usual breakpoint at the start of main, and I can continue the program (or step through) as desired. The code follows the source as expected. If at any time I continue the program, it hangs (I could post the details of exactly where here, but I'm not sure that's relevant) before entering the main while loop during peripheral initialization. I can also step into functions and find the exact spot where it hangs, which is repeatable.
So a fully functioning app that runs outside of the debugger with the ST-Link attached but inactive will start but not fully function when executed from inside Atollic using a connected ST-Link module under gdb.
Thanks for your time.
Solved! Go to Solution.
2019-10-18 1:35 AM
Hello,
I have the same problem. buy an JLINK from Segger, it is working with the BlueNRG2. It is a wonderful tool, it will save you a lot of time.
Regards,
Anthony
2019-10-18 1:35 AM
Hello,
I have the same problem. buy an JLINK from Segger, it is working with the BlueNRG2. It is a wonderful tool, it will save you a lot of time.
Regards,
Anthony
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.