Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Need details for USB Interface IC DRP

Here I'm using a USB Interface IC DRP for OTG. when I look into the datasheet for interfacing, I find some details in the pinout contrary to the diagram for pin numbers 16 and 17. Please someone clarify in this  

AravindR_0-1691125297024.png AravindR_1-1691125349801.png
Aravind R by Associate II
  • 1874 Views
  • 2 replies
  • 1 kudos

Sending data using BLEUNRG-2

Hello,I program a BLE, I can send and receive data with the ST BLE Toolbox application.I want to use another application that is not programmed by the ST community to communicate with my server, I can receive data from this application but I cannot s...

AMACH.1 by Associate II
  • 756 Views
  • 0 replies
  • 0 kudos

Resolved! TESEO LIV3F IO Supply Voltage

Hello,I would like to connect a TESEO LIV3F to an STM32 MCU that is powered using a 2.4v supply.Im wondering if I can drive TESEO's Vcc_io with a 2.4v supply or if I should use a 3.3v according to the datasheet and put a level shifter between them bo...

ABouk.1 by Associate III
  • 5649 Views
  • 10 replies
  • 1 kudos

Resolved! S2LP sniff mode

Hi,I successfully configured the transceiver RX mode with RX always ON.Now I'm trying to use Sniff mode. Basically I copied the example from S2LP DK.   // Below the code relevant for sniff mode. Initial radio, packet and address // configu...

Evgeny M by Associate II
  • 1872 Views
  • 1 replies
  • 0 kudos

BLUENRG-M2SP MAC Address issue & DTM Firmware

Hello, In one of my projects, I use BLUENRG-M2SP as a network coprocessor with a host microcontroller from STM32L0 series together. I flashed BLUENRG-M2SP with pre-compiled DTM_SPI.hex which is used by X-NUCLEO-BNRG2A1. My application code is run by ...

Blue_NRG-2 examples load but dont run

I am trying to develop some custom code using the BlueNRG-2 chip. I have my own custom board but first I am trying to get things to work on the STEVAL-BCN002V1 blue tile. That board comes preloaded with the Sensor Demo which worked fine. I am using t...

JWall.1 by Associate II
  • 919 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.