Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BALFLB-WL-08D3 with STM32WL54CC at 433MHz

Hello,i need to know if you recommend to use the BALFLB-WL-08D3 at 433MHzI design my PCB with the STM32WL54CC, and it will operate between 433MHz and 435MHz. i want to know if the BALFLB-WL-08D3 is suitable for my application or if is better to desig...

malarab by Senior II
  • 1085 Views
  • 1 replies
  • 0 kudos

BlueNRG 2

I am working with BlueNRG 2, and Tile both... I'm working in BlueNRG-1_2 DK 3.2.3. In the xx\BlueNRG-1_2 DK 3.2.3\Firmware\BLE_Examples\BLE_SerialPort\BlueNRG-2 folder, there is Server bin and hex files which work great. However, when I go to the C:\...

LPrin.1 by Associate II
  • 1033 Views
  • 0 replies
  • 0 kudos

SPIRIT1 CSMA understanding problem?

Posted on August 10, 2015 at 13:32I am performing some tests on the CSMA feature. Specifically on the non persistent CCA method. I have a test process whereby every 10s the transmitting module has its TX FIFO flushed, has its FIFO filled with 20 byt...

kzkaram by Associate II
  • 2693 Views
  • 4 replies
  • 0 kudos

S2-LP medium speed data transmission example

Hello,I'm trying to find an example project where audio was streamed using the S2LP chipset, but I can only find Sigfox/LORA examples.Do you know of any off the shelf medium speed / real-time example using the S2LP IC?  Our speed requirement is aroun...

SensorTile BLE GATT Characteristic Editing

Hi,When editing the GATT characteristic in the provided software for the SensorTile, I cannot increase the size of the payload being transmitted. Even after altering the charValueLen variable, this doesn't appear to affect the length of the packet be...

byrnep8_3-1689201716475.png byrnep8_1-1689201528729.png byrnep8_2-1689201574962.png
byrnep8 by Associate
  • 812 Views
  • 0 replies
  • 0 kudos

Should Pin 21 of BLUENRG-M2SA be grounded?

Hello,I am using the BLUENRG-M2SA in my design. In the BLUENRG-M2 datasheet at https://www.st.com/resource/en/datasheet/bluenrg-m2.pdf, it is stated that all GND pins must be grounded. However, in the BLE module integration design guidelines (DT0142)...

ASang.2 by Associate
  • 2021 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.