2023-08-01 1:53 AM
After a central device has made a succesful conection to my peripheral device (BLUENRG-LPS), I want to advertise ADV_NONCONNECTABLE / SCANABLE advertisements.
void Ble_AdvNonConnectable( void )
{
volatile tBleStatus ret = BLE_STATUS_SUCCESS;
ret = aci_gap_set_advertising_configuration(0, GAP_MODE_GENERAL_DISCOVERABLE,
ADV_PROP_SCANNABLE,
ADV_INTERVAL_MIN, ADV_INTERVAL_MAX,
ADV_CH_ALL,
0,NULL,
ADV_NO_WHITE_LIST_USE,
0, /* 0 dBm */
LE_1M_PHY, /* Primary advertising PHY */
0, /* 0 skips */
LE_1M_PHY, /* Secondary advertising PHY. Not used with legacy advertising. */
0, /* SID */
0 /* No scan request notifications */);
Advertising_Set_Parameters[0].Advertising_Handle = 0;
Advertising_Set_Parameters[0].Duration = 0;
Advertising_Set_Parameters[0].Max_Extended_Advertising_Events = 0;
if ( ret == BLE_STATUS_SUCCESS )
{
ret = aci_gap_set_advertising_enable( ENABLE, 1, Advertising_Set_Parameters );
}
}
But the peripheral device does not restart advertisements.
Solved! Go to Solution.
2023-08-01 5:47 AM
Had to set CONFIG_NUM_MAX_LINKS=2
2023-08-01 5:47 AM
Had to set CONFIG_NUM_MAX_LINKS=2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.