Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LNB Efficiency

Using the STEVAL-LNBH06 I am not able to achieve 93% efficiency as stated in the data sheet. Please advise why this might be.inout voltage: 12Vload: 43ohm power resistor for each channel (draw 420mA per channel)measured input power: 20.4Woutput power...

JAlex2 by Associate
  • 1765 Views
  • 2 replies
  • 0 kudos

NUCLEO-H743ZI2

Hello Everyone!I think it's a weird question, however, I am new to NUCLEO-H743ZI2.  Actually, I am facing the issue of low-speed data transfer from MCU to PC (LabVIEW). Before, I was using programming and debugging USB ports to transfer data to LabVI...

LIN transceiver

Hi team,Is there any transceiver that has 2 channels and is ISO14230 or ISO9141 compatible? The most important is that this transceiver must supports 24 V in VBB pin (vehicle batery). Also is important that there is a level changer internally.

Aarong by Associate
  • 1068 Views
  • 0 replies
  • 0 kudos

L9369 getting voltage from SH1, SH2

Hello. ST team.i'm using L9369's voltage measurement function.i read L9369 manual, and i send below SPI commands(no.0~6) for initial driving.(my purpose is to drive FET : HS1 A, B ON / LS2 A,B ON)00xb5019ff810xb5a15fef20xb720b54d30xb480aa9840x40a0000...

ldong.1 by Associate III
  • 1548 Views
  • 1 replies
  • 0 kudos

LVDS transceiver RHFLVDSR2D2 failure info

Good afternoon, We are evaluating the possible consequence for the LVDS transceiver RHFLVDSR2D2 in case that it is supplied with a voltage above its absolute value which is 4,8V.In particular we are asked to evaluate the case that voltage applied to ...

Capacitive SENSOR with STM32

Hello to everyone. I am trying to see the data via I2C with the capacitive sensor (FDC2214-Q1),but I see the values I have assigned as 0 in live experiment.I'm sure about the hardware part. I would be happy if you help.  /* Private define -----------...

MDaya.2 by Associate II
  • 2074 Views
  • 2 replies
  • 0 kudos

STUSB4500L USB2.0 data communication

Hi ST community,does the STUSB4500L also supports negotiation for data communication?E.g. can I use D+/D- pins of the USB-C port while PD is negotiated by the STUSB4500L?The STUSB4500 seems to support that by setting the flag USB_COMM_CAPABLE within ...

mk279 by Associate
  • 900 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.