Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STUSB4500L Logic Voltage

I am wondering what the logic voltage is for the I/O pins on the STUSB4500L. Under operating conditions they are listed as 0V to 4.5V, but the example circuit shows I2C pullup resistors to 3.3V. Is it safe to connect these I/O pins directly to a 3.3V...

S2-LP DK wrong firmware

Hi,I am trying to use S2-LP DK with a Nucleo + S2-LP Shield. I tried several combinations (4 computers (Windows 10), 6 Nucleo Boards (STML053 and STML152) and 4 S2-LP shields, S2-LP DK V1.2.0, 1.3.0, 1.3.2), I always get the error that I have the wro...

TKlei.7 by Associate
  • 1032 Views
  • 1 replies
  • 0 kudos

Failed to execute MI command: Cannot access memory at address 0xffffffbc

After closing serial port, when i re-open serial port with the updated baud rate, I'm getting an error:  Failed to execute MI command:          -data-disassemble -s 4294967228 -e 4294967330 -- 3          Error message from debugger back end:         ...

[BLUENRG-LP] Scan devices when using CODED_PHY

Hello everyone. I'm facing a issue when I try to use CODED_PHY instead 1M_PHY. When I start a GAP_GENERAL_DISCOVERY_PROC, the stack returns: 0xD1 (BLE_STATUS_INVALID_SCAN_CONFIGURATION).Could anyone help me? The scan configuration is (return 0x00 - O...

LTrin.1 by Associate II
  • 1020 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.