2023-09-25 11:53 AM
Using the STEVAL-LNBH06 I am not able to achieve 93% efficiency as stated in the data sheet. Please advise why this might be.
inout voltage: 12V
load: 43ohm power resistor for each channel (draw 420mA per channel)
measured input power: 20.4W
output power: 17.2W
efficiency: 85%
2023-09-25 3:02 PM
2023-09-26 6:12 AM
Are you referring to where it specifies Iout as 500mA? If so, I have already tried this condition on the evaluation board even with low power mode active, and only improved to 87%. Please advise what condition you are referring to if this is not it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.