2023-09-09 10:28 PM
Hello. ST team.
i'm using L9369's voltage measurement function.
i read L9369 manual, and i send below SPI commands(no.0~6) for initial driving.
(my purpose is to drive FET : HS1 A, B ON / LS2 A,B ON)
| 0 | 0xb5019ff8 |
| 1 | 0xb5a15fef |
| 2 | 0xb720b54d |
| 3 | 0xb480aa98 |
| 4 | 0x40a0000d |
| 5 | 0xbb8020ea |
| 6 | 0xc3a000f5 |
after sending above SPI commands to check SH1/2_A/B's voltage AD read.
| 14 | 0x0c20001f |
| 15 | 0x0d000010 |
| 16 | 0x0e200001 |
| 17 | 0x0f00000e |
| 18 | 0x1020001a |
| 19 | 0x1620001d |
| 20 | 0x17200012 |
| 21 | 0x1800000d |
| 22 | 0x19200002 |
| 23 | 0x1a000013 |
| 24 | 0x11000015 |
| 25 | 0x12200004 |
| 26 | 0x1300000b |
| 27 | 0x14200003 |
| 28 | 0x1500000c |
| 29 | 0x1b00001c |
| 30 | 0x1c200014 |
| 31 | 0x1d00001b |
| 32 | 0x1e20000a |
| 33 | 0x1f000005 |
after sending above SPI commands, i checked measured data, but the measured voltage is approximately 0.6V lower than the actual measurement value obtained through the oscilloscope.
After completing the above operation, I send the following SPI commands(no.7~13) again.
(my purpose is to drive FET : HS2 A, B ON / LS1 A,B ON)
| 7 | 0xb5019ff8 |
| 8 | 0xb5a0bfea |
| 9 | 0xb7015548 |
| 10 | 0xb4a0aa98 |
| 11 | 0x4080000d |
| 12 | 0xbba020ea |
| 13 | 0xb401994d |
After sending above SPI commands(no.14~33), i measure SH1/2_A/B's voltage again.
In the second operation, I confirmed that the values measured with the SH pin's AD value and those measured with the oscilloscope were nearly same.
My question is this: Why is the voltage output approximately 0.6V lower in the first operation? What SPI settings do I need to configure? (All four ACT_OFF_LS pins are in a low state after the first operation, switched to a high state to stop the H-bridge after the first operation, and then switched back to low just before the second operation to enable the H-bridge again.)
please let me know. thank you.
2023-09-14 10:07 AM
Hi ldong.1,
This question has been routed to the online support center for direct support by our specialist team. Please check your account for updates and support regarding this request.
Regards,
Jake
ST Support
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.