2023-09-25 6:02 PM
Hello Everyone!
I think it's a weird question, however, I am new to NUCLEO-H743ZI2. Actually, I am facing the issue of low-speed data transfer from MCU to PC (LabVIEW). Before, I was using programming and debugging USB ports to transfer data to LabVIEW. However, I was only able to transfer at a maximum of 115200bps (14400 Bytes ps). Although my requirement is 50,000 Bytes per sec.
Then I found the USB OTG_FS Connector (CN13). However, I am not sure about the maximum speed through which I can transfer data. And what about the Ethernet port (CN14)?
2023-09-25 6:48 PM
The UART port should be capable of 921600 or more. Increasing baud rate is probably the easiest solution here.
USB FS can transfer around 5 Mbps, but is more complicated to program.
Eithernet faster than USB FS, unsure of the max but at least 10s of Mbps.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.