Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Perform HTTP delete, put

Posted on July 13, 2016 at 14:56Is it possible to perform a HTTP DELETE or HTTP PUT through the AT commands (without opening socket etc.). Is it possible using the custom request command  AT+S.HTTPREQ? I have found no example of how to use  AT+S.HTT...

pontus2 by Associate II
  • 987 Views
  • 1 replies
  • 0 kudos

Spirit1 STack packet ACK - what is it?

Posted on July 14, 2016 at 20:18While I await some expert help on the question about a packet sniffer for the STack protocol, can anyone describe what is the ACK in the STack protocol? What does it look like (i.e. does it have a preamble and/or sync...

SPIRIT1 STack problem

Posted on February 23, 2015 at 12:20Hello, I am currently testing the code examples provided with the SPIRIT evaluation kit. (the kit used is STEVAL-IKR002Vx). The exmple name is ''StackGeneric''. The behaviour is, quite weird. Indeed, when I send 3...

Spirit1 STack packet mode sniffer?

Posted on July 14, 2016 at 20:16How can I configure the ST DK eval from the SPIRIT1 DK GUI Application v2.2.0 to properly sniff packets that are sent using the STack packet mode? I have implemented my system from a sample app and tuned it using the ...

Spirit1 STack packet mode fixed length?

Posted on July 13, 2016 at 03:49I am trying to configure for STack packet mode using fixed length packets with 4 preamble 4 sync 1 dst addr 1 src addr 0 control 80 data 2 crc The total of above is 92, but data sheet says the length is only inclusive...

SPWF01SA.11 firmware downgrade

Posted on June 15, 2016 at 15:22Hello, I wrote my software with SPWF01SA.11 Version 140805-3f58d6b to use it as a mini-webserver linked to a wifi router (wifi_mode = 1, no dhcp). My code is working well with this item. Now, we received new modules S...

be by Associate II
  • 1700 Views
  • 4 replies
  • 0 kudos

SPWF01Sx client- server

Posted on July 05, 2016 at 09:41Hi I have two SPWF01Sh device is installed between the communication method ofserverAT + S.SSIDTXT = SPWF_APAT + S.SCFG = wifi_priv_mode, 1AT + S.SCFG = wifi_wep_keys [0] 7465737431AT + S.SCFG = wifi_wep_key_lens, 05A...

baf00 by Associate
  • 979 Views
  • 2 replies
  • 0 kudos

SPSGRF-868 Narrow Range

Posted on July 04, 2016 at 14:00We are using SPSGRF module in one of our projects. We are not really pleased with the range of this module. So far the best range we could get was less than 1 m. We are using the P2P demo software Please see below the...

Pradeep1 by Associate
  • 636 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.