Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

+WIND:30:WiFi BSS Lost

Posted on July 22, 2016 at 16:10Hello, While doing my PoC on the Wifi module, I see the following messageson the console  : +WIND:30:WiFi BSS Lost +WIND:14:WiFi BSS Regained (0) So far, I understand that's a loss of communication with the WiFi AP. S...

BlueNRG showing no service

Posted on July 05, 2016 at 16:57Hi All I'm using the BlueNRG Chip together with the LightBlue iOS app. I was able to set up 2 services (Device Information and Battery Service). However the LightBlue app states ''No Service'' but when I connect both ...

0690X00000604x1QAA.png
b_ by Associate II
  • 1011 Views
  • 1 replies
  • 0 kudos

X-Nucleo-IDB04A1 interface STM32F217

Posted on July 25, 2016 at 07:57Hi,I want to interface X-Nucleo-IDB04A1 (BlueNRG) with STM32F217 (using STM3221G Eval board). I have used the SensorDemo in X-cube-ble1 (for X-Nucleo-IDB04A1 and Nucleo-L053R8 ) and I have re-adpated the files to be c...

BlueNRG SPI not ready

Posted on July 15, 2016 at 15:09HelloI use a BlueNRG with a STM32F302x8. To test the SPI I use the AN4494 and it works fine. After a BlueNRG reset I read a Blue_Initialized_Event (04 FF 03 01 00 01) by using an interrupt on SPI_IRQ and the function ...

UDP receive issue

Posted on July 05, 2016 at 11:06Hi,I can't receive the UDP packets sent from SockTest (SERVER) to the Wi Fi module (CLIENT).I connect the Wi Fi module via TeraTerm, configure it and then sent an ''AT+S.SOCKON=192.168.32.255,4999,u,ind'' to prepare t...

scash9 by Associate
  • 2117 Views
  • 3 replies
  • 0 kudos

SPBT2632C2A fixed pin code for pairing

Posted on July 20, 2016 at 18:16HelloI need help pleaseI use a SPBT2632C2A Bluetooth module with an arduino nano. I use both for sending sensor data to an application on an android tablet.All work well but I can not find how to set a FIXED PIN code ...

ERROR: Unable to load CA certificate

Posted on July 17, 2016 at 12:35Hello, Doing the Example 1 of the AN4683 (TLS Example 1, mutual auth), all commands work without problem (keys and certificate generation), same for imports in Wifi module (send back ''OK'') But the last command : AT+...

Is there a way to speed up VCOM?

Posted on July 19, 2016 at 19:45When monitoring the SPI bus on the IDB002V1, I notice that polling stops for 3 to 6 mS every time a Command Complete Event is received.  This slows down how fast we can send commands to the BlueNRG.  Is there any way ...

rdscliff by Associate II
  • 649 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.