Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG spi is not ready

Posted on August 31, 2014 at 12:45In our device, we use BLUENRGGCSP module (marking on the chip: BLUENRG AZ 001  P6 TW 4 18) in WLCSP34 package. We also have BlueNRG Eval Kit.  In our device and in the Evaluation board, we use the same firmware (blu...

Secure authentication to web server

Posted on June 15, 2016 at 13:15Hi to all, I've created simple dynamic webpages using CGI and SSI provided by the wi-fi module. The pages are stored in the external flash of the SPWF01SA module and it works well. Now I would like to add authenticati...

tabekb by Associate III
  • 711 Views
  • 1 replies
  • 0 kudos

HTTPPOST Example Android GCM

Posted on March 23, 2015 at 13:57Hi All, I'm evaluating the SPWF01, so I want to send an Android GCM HTTP post (json or plain text) - but I've no success. I tried it with: AT+S.HTTPPOST=android.googleapis.com,/gcm/send,Content-Type:application/x-w...

Connecting SPWF01S using WPS

Posted on June 27, 2016 at 13:52Hello!Is there a way to connect to an existing AP without hardcoding the SSID, login credentials etc? For example, using WPS. In the AT command spec there is a Table defining some errors where number 21 has the messag...

pontus2 by Associate II
  • 661 Views
  • 1 replies
  • 0 kudos

Trouble connecting to AP (using WPA2)

Posted on June 28, 2016 at 16:25I am trying to connect my SPWF01S to an AP but am not able to do so. This is the WINDS i get:+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:19:WiFi Join:74:EA:3A:D3:C4:D4+WIND:25:WiFi Association with 'I...

pontus2 by Associate II
  • 916 Views
  • 1 replies
  • 0 kudos

Missing Discrete Balun Values

Posted on July 03, 2016 at 01:55Hello,Kindly advise with the exact discrete balun values in the following document, page7:http://www.st.com/content/ccc/resource/technical/document/application_note/b7/1b/cd/46/3b/a8/46/81/DM00150501.pdf/files/DM00150...

moataz by Associate
  • 544 Views
  • 0 replies
  • 0 kudos

BlueNRG MS only connects to random addresses

Posted on July 01, 2016 at 00:54Hi,I am rather new, although advancing in big steps with through the blueNRG chips, which i find the be really great!I am runing latest FW version, and i noticed something rather strange:If my central device has a ran...

ika by Associate
  • 677 Views
  • 0 replies
  • 0 kudos

BlueNRG-MS Count of Services? Only 6?

Posted on June 29, 2016 at 14:46Hello, after adding the 6th service with aci_gatt_add_serv i get the errorcode 0x1f (out of memory) if i add the 7th service? This error is independent of the count of characteristics in the other services. How can i ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.