2016-07-01 2:38 AM
Working with the SPWF01SA.11 module. In an attempt to make my program event based, I was trying to utilize the indications for reading data received from a socket. But I am not getting the +WIND:55 indication although data is received:
1. Open a socket to a MQTT server (test.mosquitto.org) -> OK2. Send a MQTT CONNECT packet -> OK3. Wait for +WIND:55:Pending Data10 seconds goes by with nothing at all received from the WiFi module4. Close the socket -> ERROR: Pending data5. Query pending data -> DATALEN: 46. Read four bytes -> Get exactly the response I was waiting for.Same as a communication log:AT+S.SOCKON=test.mosquitto.org,1883,t ID: 00OKAT+S.SOCKW=01,36Send 36 bytes of socket data.OKAT+S.SOCKC=00ERROR: Pending dataAT+S.SOCKQ=00 DATALEN: 4OKAT+S.SOCKR=00,4Read 4 bytes of socket dataOKWhy am I not getting the indication? None of the indications is disabled.The version date of the module was 150410, and since the ST website has a newer version 160129, I decided to update. The batch file in the update packet - after inputting the .bin file path and the serial port number - takes about an eyeblink to run to 'Press a key to exit...'. It gives no error messages, but obviously does not update the firmware either.It does print a web address which lead me to Sourceforge stm32flash page. I downloaded that program and ran it instead of 1203flash.exe used by the batch file. I used exactly the same command line arguments, and this time the binary file was programmed to the module. Only, now the module is dead. How do I recover it?The new version would be useful also because it supports error numbering in the ERROR response. Parsing the error code form the description string is unnecessarily tedious.2016-07-04 2:14 AM
If you need the indication, turn the indication on.
AT+S.SOCKON=test.mosquitto.org,1883,t,indAbout the stm32flash, I think you deleted the bootloader. Module is lost. Contact your direct support/distributor to get a recover image...2016-07-04 4:41 AM
Ahh, I somehow managed to miss that ind. I didn't realize that you can control it by socket.
About the recovery image.. Should I program it with stm32flash? And why didn't 1203flash work? Do I ever again dare to try update the module firmware?2016-07-05 4:43 AM
You can use stm32flash (the one given by ST, not the standard one from Google code) or STM32 Flash Loader Demonstrator. Contact ST to recover dead module
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.