2016-07-05 2:06 AM
Hi,
I can't receive the UDP packets sent from SockTest (SERVER) to the Wi Fi module (CLIENT).I connect the Wi Fi module via TeraTerm, configure it and then sent an ''AT+S.SOCKON=192.168.32.255,4999,u,ind'' to prepare the Wi Fi module to listen for udp packets.Now, from SockTest, I sent a message to 192.168.32.255 (or the specific IP of theWi Fi module) / port 4999 but I don't receive nothing (I should receive the WIND:55 indication).I try to test even with the CubeExpansion WIFI1 V2.1.0 - Client_Socket firmware for IAR, the sent function is OK but I can't receive the message from the Server (SockTest ) on the Wi Fi Module.I only change the protocol from ''t'' of TCP to ''u'' UDP.If I use the with TCP protocol it work well.I need to have the UDP packets receive.The FW is 160129-c5bf5ceRegard.Stefano.2016-07-05 4:52 AM
SOCKON configures a socket client (connect), SOCKD opens a socket server (listen).
- Open SockTest (server)- Call SOCKON (client) -> since UDP, traffic is not generated, ans, so, ''connection'' is not performed since at least 1 packet sent/received- Call SOCKW to send a packet -> now ''connection'' is created- Send packets from SockTest to moduleAs an alternative, call SOCKD on module, and use SockTest as client2016-07-05 6:44 AM
The problem is I am trying to put the module Wifi to listen the broadcast messages in UDP, no mater who is sending my task is to send and receive broadcast messages in or from UDP. I have tried to make UDP server with Wifi module and tried to communicate with a simple client and it works but if I try to make my wifi module listen to the broadcast messages passing in network then it doesnt receive anything at all.
2016-07-21 11:35 PM
Ciao Stefano,
can you share your test case? Mainly AT-Commands used.Please remember, if you are using socket server, that it's able to manage only one connection at a time. Doesn't matter if unicast or broadcast. In this case, when a connection is established (even if UDP), other incoming packets are discarded.RegardsjWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.