2016-07-22 7:10 AM
Hello,
While doing my PoC on the Wifi module, I see the following messageson the console : +WIND:30:WiFi BSS Lost +WIND:14:WiFi BSS Regained (0) So far, I understand that's a loss of communication with the WiFi AP. Sockets get 1/2 closed (can't be used, but not closed) and I get the mess in communication. I have not found any mean to improve the situation. Two questions : - What are the possible causes of the messages Wind 30 / 14 ? - What can I do to improve the situation ? Thanks a lot Zirco2016-07-27 2:10 AM
Hi Zirco,
BSS loss/regain are indication not relevant at production stage. Use wind_off_xxx variables to mask them.Please note that BSS loss/regains doesn't means loss of connection with AP. When connection is lost, +WIND:33:WiFi Network Lost is raised after a BSS loss (not regained!). When a regain is not reached within 2 seconds from BSS loss, then WIND:33:network is lost.Further info: you can delay BSS loss notification through wifi_beacon_loss_thresh configuration variable (0 means: never raise BSS loss). This variable set the number of ''accepted'' consecutive beacon lostRegardsjerryWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.