Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Custom response headers for *.cgi scripts/pages

Posted on August 24, 2016 at 03:15Our customer has requested that our device using the SPWF01SA use modified http headers in the response for the firstset.cgi page. Is there a way to modify the headers?  Perhaps a special file in the filesystem that...

ccarlsen by Associate
  • 883 Views
  • 1 replies
  • 0 kudos

How to get max WIFI speed performance on SPWF?

Posted on August 22, 2016 at 10:50Hello! I'm building the system with cooperation of Host MCU - SPWF at one side and PC with client-program at the other side. They are in the same LAN and they communicate through wifi router. SPWF is a TCP-server an...

daniil by Associate II
  • 1824 Views
  • 3 replies
  • 0 kudos

mini AP help

Posted on August 15, 2016 at 16:48I'm finding very little info on how to set up the module.  Can anybody point me to some sample scripts or something?   My goal is to see the SSID with a phone/tablet/laptop and connect to it and then open a webpage ...

pmuldoon by Associate
  • 1070 Views
  • 1 replies
  • 0 kudos

Module UART RX buffer

Posted on August 12, 2016 at 08:17I cannot find information on the SPWFS01 UART RX buffer. How big is it? Since I have an issue when controlling the SPFWS01 from a host using UART. We have a cycle where we use HTTPREQ and in there use GET, PUT and t...

pontus2 by Associate II
  • 964 Views
  • 1 replies
  • 0 kudos

Connection to UART for a beginner

Posted on August 10, 2016 at 14:14Hello everyone ! I'm sorry about those dumb questions, but I just began my internship 2 days ago in a company that wants to work with the SPWF01SA module. They gave 2 boxes and no explanation. And the guy who used t...

Perform HTTP Get with listed parameters

Posted on August 11, 2016 at 09:40I need to perform an HTTP Get request to a server that supports listed parameters, an example being:myshop.com/storesrequest.aspx?userid=1234&zipcodes=123,456,789As you can see the zipcodes parameter supports a list...

justin23 by Associate II
  • 1366 Views
  • 2 replies
  • 0 kudos

AT+CFUN=1 unexpected reaction on ver 3.5 of FW

Posted on July 27, 2016 at 06:31Hello! I have some troubles with wifi module. At first I have upgraded a firmware of my SPWF01SA.11from ver 3.3 (default) to ver 3.5 following instructions. And since this moment I found unexpected reaction of module...

daniil by Associate II
  • 1643 Views
  • 1 replies
  • 0 kudos

STW81200 Phase control

Posted on July 29, 2016 at 11:28Hi,I am currently using STW81200 Synthesizer in integer mode.I am wondering if there is a way to use fractionnal mode features (such as the DSM) to control the VCO relative phase to the reference input?This is somethi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.