2016-07-24 10:57 PM
Hi,
I want to interface X-Nucleo-IDB04A1 (BlueNRG) with STM32F217 (using STM3221G Eval board). I have used the SensorDemo in X-cube-ble1 (for X-Nucleo-IDB04A1 and Nucleo-L053R8 ) and I have re-adpated the files to be compatible with STM3221G Eval board, that is the port mapping and all drivers, I run the code and i find no errors. I load the application and I get nothing when testing with my Android phone 4.4 (BLE compliant). Could anybody give me some tips on how I can work this around? ThanksSteps I have taken into this approach:1- Connect the pins to Corresponding SPI pins2- Include all drivers for the STM32F217 to be recognized by the compiler3-add lines to USE the STM322xG_Eval in all relevant files (C and h)4-Check relevant include paths, and files5- Build all target (no errors) and load #stm32f217 #x-nucleo-idb04a1We’re moving the ST Community to a new platform to give you a better and more reliable community experience.