cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF0SA21 - +WIND:45:Dot11 AuthIllegal 28679/55

Andre Petronilho
Associate
Posted on December 20, 2017 at 18:55

I was using a SPWF0SA11 module in my application and it was working fine, when I changed to the production PN, that is SPWF0SA21 I am not able to connect to the module in MiniAP mode. The following message is received from the module:

+WIND:2:Reset

+WIND:1:Poweron (170111-665d284-SPWF02S)

+WIND:13:STM SPWF01SA21 IWM: Copyright (c) 2012-2016 STMicroelectronics, Inc. All rights Reserved.

+WIND:3:Watchdog Running

+WIND:0:Console active

+WIND:32:WiFi Hardware Started

+WIND:26:WiFi Started AP with network 'CERVEJEIRAMEMO'

+WIND:24:WiFi Up:172.31.141.1

+WIND:45:Dot11 AuthIllegal 28679/55

+WIND:45:Dot11 AuthIllegal 37612/237

+WIND:45:Dot11 AuthIllegal 37614/239

The mobile that is trying to connect to the module show an message that authentication was not possible.

with the 

SPWF0SA

1

1 module the message that I receive from the module when mobile connects is:

+WIND:28:Station 30:07:4D:82:72:50 Associated

+WIND:29:DHCP reply for 172.31.117.2/30:07:4D:82:72:50

Please Help, this is urgent. Product is going into production soon.

I am also attachign some logs with dump configuration from both modules.

Thanks

#+wind:45 #spwf0sa21
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andre Petronilho
Associate
Posted on December 20, 2017 at 19:42

One additional information is that the Firmware version on the module that is working is much older than in the module that is not working. It is possible to see version on the attached logs.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.