Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Overall impression of SPIRIT1 radio ICs ?

I have been attempting to use Silicon Labs Si443x/RFM22 ISM radio IC for over a week now with no success. My overall impression of this radio IC is poor. Lots of issues, erratas, and twitchy-spazz operation even under ideal conditions. So naturally I...

gahelton1 by Associate III
  • 1013 Views
  • 1 replies
  • 0 kudos

S2-LP 403MHz

Hi All, Currently S2-LP only supports down to 433MHz, would it be possible to use a lower frequency crystal to achieve a lower frequency such as 403MHz?Thanks!Xarion

xarion by Associate II
  • 758 Views
  • 0 replies
  • 0 kudos

Problem with AT+S.HTTPDFSUPDATE for SPWF01

Hello allI have a problem with updating the filesystem over httpAT+S.HTTPDFSUPDATE=192.168.3.2,/fs.img,8079this is the command i use to update the fs.The logs of the local webserver tell192.168.3.1 - - [14/Jan/2019:13:29:51 +0300] "GET /fs.img HTTP/1...

Z.Oleg by Associate II
  • 2273 Views
  • 4 replies
  • 0 kudos

How to evaluate performance of bluetooth mesh network with STEVAL-IDB007/8 boards and a smartphone ?

Hello @alok​ , @STM Community​ , @Jitendra J_O​ ,I want to evaluate the performance of bluetooth mesh network having 4 mesh nodes (3 provisioned STEVAL boards and one smartphone). Which parameters can I measure on STEVAL board in order to evaluate th...

MH1 by Associate II
  • 3113 Views
  • 6 replies
  • 0 kudos

SPBTLE-1s Example Project Run

Hello, I am evaluating SPBTLE-1s module. I am working on a example project provided by the BlueNRG-1_2 DK 3.1.0 (remote control). The project build on truestudio and is burned on chip via st link utility. Application success messages prints on the se...

SPWF01SA Wind:5: Hardware Failure: 5

Hi everyone,Sometime when I try to connect the module to a exsisting WiFi network I receive the following string from the module:+WIND:0:Console active+WIND:32:WiFi Hardware Started+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0xFF)+WIND:5:WiFi ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.