2019-01-07 10:18 AM
Hello,
I am evaluating SPBTLE-1s module. I am working on a example project provided by the BlueNRG-1_2 DK 3.1.0 (remote control). The project build on truestudio and is burned on chip via st link utility. Application success messages prints on the serial terminal but no module is discoverable on my android phone. I'm using BlueNrg android app.
Note: for Spbtle-1s i have changed the preprocessor macro from 16MHz external clock to 32MHz.
Thanks.
2019-01-12 11:01 PM
Kindly try another project like Beacon, which is simple to test
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.