how to measure the RSSI value of the beacon demo without the smartphone
i want to know how to measure the RSSI value of the beacon demo without the smartphone.is it possible? if yes , which function can i use?thank you
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
i want to know how to measure the RSSI value of the beacon demo without the smartphone.is it possible? if yes , which function can i use?thank you
Posted on January 07, 2018 at 03:06Hi, I just got the EVAL-IDB007V1M with the spbtle-1s (based on bluenrg-1 and installed the STSW-BLUENRG1-DK (v2.5.0) on my Windows PC. The BlueNRG-1 Navigator recognizes the EVAL-IDB007V1M and I can 'Flash & Run' t...
Hi, Could someone walk me a quick through what the difference between STEVAL-IDB008V2 and STEVAL-IDB008V1? The STEVAL-IDB008V2 is a newer version evaluation kit for BlueNRG-2 over STEVAL-IDB008V1, but what is the essential change? Especially for f...
How to setup STUSB4500 to deliver 15V 2.5A without programming ?If programming needed, how it can done?Where should I get the evaluation board for the same?Can I power STUSB4500 using the charging port without connecting to battery(Powered from Sourc...
Hi everyone,I have got some problems with programming SPI between ADE7758 (slave) and STM32F103C8 (master). I use build - in SPI (hardware SPI), and directly connect 4 pin (MOSI, MISO, NSS, CLK) to ADE7758 which is a 5V device without any conversion ...
Hi I am using parallel bus to communicate with the OLED SSD1322 to display something, which include: DATA LINE0 to LINE7CSRDWRDM data or commandhowever , I could send the simple commands like display on , off to control the OLED after initializatio...
Hi all,using the STEVAL-PCC009V2 demo board I've connected an external EEPROM 24LC02 to this board by means of the I2C1 peripheral through the lines PB6 (SCL) and PB7 (SDA), these lines are available through the connector J2 (30 pin connectors on boa...
I need to build a device with the Home Automation Profile (HA 1.2) . I would need help in order to select the proper Wireless MCU that could have the corresponding libraries and Zigbee Stack. Selection of the proper MCULibraries for that MCU with the...
iPhone 7, OS vesion is 12.0. BlueNRG-2 is first time used. iPhone can't find it, but when I use Andriod phone, it can find the BlueNRG-2. Whatis happen?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.