Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to transfer audio files from the phone to a (BLUENRG+STM32+SDcard), without using additional software on the phone?

How to transfer audio files from the phone to a (BLUENRG+STM32+SDcard), without using additional software on the phone? I'm not sure, but I need an FTP profile. I need to realize the transfer of a sound file using the built-in Android / IOS functions...

Upadate BlueNRG firmware using SPI and STM32

Hi,I have a BlueNRG-MS connected through SPI to a STM32L476 like that implemented on ST SensorTile board. The NRG chip wasn't working and I checked that the firmware version is 715. I think 723 is a the latest version and so I am trying to update the...

Resolved! STEVAL-FKI868V1has feature'Automatic acknowledgement, retransmission, and timeout protocol engine'. Does this feature automatic for S2-LP transceiver or it may be enabled/disabled programmatically?

S2-LP transceiver, STEVAL-FKI868V1: it has a feature 'Automatic acknowledgement, retransmission, and timeout protocol engine".1. Does the acknowledgement automatically come from receiver?2. Does this feature automatic for S2-LP transceiver or it may ...

bvn123 by Associate II
  • 1931 Views
  • 3 replies
  • 0 kudos

Resolved! Connecting Bluetooth HID keyboard to STM32

Hi,I'd be grateful for any suggestion what BT module supporting HID I should use to connect BT HID keyboard to the STM32. I see that many popular HC-XX modules support only SPP profile.There are some modules supporting HID profile but all the example...

HAL_I2c_Mem_Read() failed

Hi,I'm using HAL_I2c_Mem_Read(), too.And may I ask if STM32's I2C can generate wave like the following picture. I have tryed Mem_read() and any other function in i2c.c , but the bit following device addres is "0",which means "write" in I2c.eg.I want ...

0690X000006D8D0QAK.jpg
dbo by Associate II
  • 1272 Views
  • 2 replies
  • 0 kudos

Sending Data between QI Devices

I've bought two ISB042V1 and i want to send sensor Data trough the QI connection from the Rx to Tx. But i do not understand how i can write data from MCU1 into Rx device, and read out from Tx device into my MCU.

roku by Associate II
  • 730 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.