is it possible to connect stm32 microcontroller with rtl8201f network ethernet ic
I dont know how i should connect stm32 with rtl8201f wich serial communication should i useuart or spi or 12c ????
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
I dont know how i should connect stm32 with rtl8201f wich serial communication should i useuart or spi or 12c ????
Hi,I am at a complete loss, so I would really appreciate any direction you could give me.I have bought a STEVAL-IDB011V1 evaluation board for the BlueNRG-LP and I would like to edit / extend one of the example applications. But this is my first time ...
After the call returns BLE_STATUS_SUCCESS, but the target BLE Peripheral slave device stops advertising forever (i.e. a race between scan result, connection request and peripheral stop advertising/go out of range)?It would be nice if a connection req...
Hi,I'm trying to configure my STUSB4500 by following the STSW-STUSB002 quick start guide.I have everything ready except for the NUCLEO-F072RB board.Instead, I have Nucleo-H743ZI2 and the STM32F769 Discovery board, but I'm pretty sure I can't just dr...
Do we need to do a software reset or any additional function in order to trigger the downstream device to adjust their sink settings and reset the power contract that is in place? Or is the power contract automatically renegotiated when the POD curr...
I have connected Stm32f407 discovery board with Simcom A7670 via USART6 but in asynchronous mode, connecting UART Tx of A7670 with USART6 Rx of STM43f407 discovery board and UART Rx of A7670 with USART6 Tx of STM43f407 discovery board respectively. ...
Hello, I hope this post is in the right place.I've been trying for a while to integrate an ATWINC1500-MR210BP module in my custom board with a STM32L151VeT6. Project is done with STM32CubeMX and later with STM32Cube IDE. For debugging purposes I am o...
Hi,is there any example project of how to implement a BLE Eddystone beacon?Best,Nikos
Hello ST/Forum,I have a design where there seems to be confusion surrounding the inductor values and names:In the "PCB design guidelines" the inductors are name L14, L13 and L6.However, in the codebase, the inductors are called "RM1" and "PMU" induct...
Hi community.I'm new in the world of bluetooth and I need some help with blueNRG modules.A few days ago, I was looking for a bluetooth module for my proyect and I found the blueNRG-1/2/ms.. but i've a problem, i don't know how calculate all necessary...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.