Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [SOLVED] DTM_SPI software for BlueNRGM2SP chip on X-NUCLEO-BNRG2A1 is not working at all.

Hello to all,I succesfully upload the DTM_SPI firmware on my X-NUCLEO-BNRG2A1 board, , using the SWD, but the BLE chip is no more responding. I'm using the X-NUCLEO-BNRG2A1 with a STM32L476RG-Nucleo, and I tried the "SampleAppThT" application to set ...

clemente by Associate III
  • 2769 Views
  • 4 replies
  • 0 kudos

BLUENRG-232_SCH_REVA_30JUNE2020

hi,We designed a board using BlueNRG-2 and we uploaded the GPIO demo code available in BlueNRG-2 navigator (to toggle DIO14) to the board using the BlueNRG-ST- Link utility. The board didn't detected with high Frequency(.9MHz-4Mhz) so we changed the ...

RJOY.1 by Associate III
  • 1611 Views
  • 1 replies
  • 1 kudos

S2-LP CSMA feature in transceiver mode

Hi,I am trying to implement CSMA feature on S2-LP. I am working with SDK_Csma_X examples. The SDK_Csma_A example is a transmiter and the SDK_Csma_B is receiver. I have to have the transceiver. When I combine the two examples there is no acnowledgemen...

lukasz2 by Associate III
  • 870 Views
  • 0 replies
  • 0 kudos

BLUENRG2 SW GUI with custom board

Hi, I'm using Bluenrg2 chipset on a custom board and bluenrg (UART pins) is connected to the PC via USB-2-uart connection. Is this okay? What is the requirement to connect Bluenrg SW GUI with custom board without STM32With the above mentioned connect...

sg.14 by Associate
  • 1198 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.