Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using the VL53L1x API with the controller that I use

I am using a TI simplelink controller. How do I go about using the VL53L1 APIs with my controller code. I am guessing I need to use STSW-IMG007 software. I can't use this software directly. How should I go ahead with interfacing it? Any guidance will...

VBhag by Associate II
  • 1633 Views
  • 2 replies
  • 0 kudos

X-NUCLEO-6180A1 GUI Crashing when trying to calibrate

Hi, I am trying to use the X-NUCLEO-6180A1 GUI to perform a offset and x-talk compensation calibration. Something i get the offset one to complete, and others times I don't and then the x-talk one will not complete. It just seems to hang up in the mi...

RHill.4 by Associate II
  • 2580 Views
  • 2 replies
  • 0 kudos

X,Y and Z coordinates for X-NUCELO-53L1A1 TOF sensor.

Hello everyone,so I am using the X-NUCLEO-53L1A1 TOF sensor and I want to detect the height ( Z) of objects that it detects but in the examples I found it only shows information about the objects' range ( distance Y) so my question is : Is there a w...

WYous.1 by Associate III
  • 6436 Views
  • 7 replies
  • 0 kudos

Why I can't get vl53l0x to work with RAK3172?

Hello guys, I am trying to use VL53L0X with old version of VL53L0X API (There is an issue with new version aapi with windows.h). Status always returns -20. Why is that? My Code;/* USER CODE BEGIN Header */ /** **************************************...

I wanted to insert a ToF sensor (VL53L4CD) in an anesthetic container, I wanted to know which types of glass are suitable with the sensor.

I wanted to insert a ToF sensor (VL53L4CD) in an anesthetic container, because of the influence of the anesthetic on the sensor I need to protect my sensor with a protective glass, I wanted to know which types of glass are suitable with the sensor (c...

kdass.1 by Associate
  • 1582 Views
  • 2 replies
  • 1 kudos

Do all VL53L* sensors use the same VCSEL with the same power?

I was wondering if all the VL53L* sensors use the same VCSEL illumination source with the same average and peak power. I would think the the long-range sensors (VL53L1CB) and the sensors with wide FoVs of 63 degrees, would need a more powerful VCSEL.

FGuti.2 by Associate II
  • 1231 Views
  • 1 replies
  • 0 kudos

Sensor init failed on using VL53L1X ultra low power driver

We have been using the full driver for VL53L1X and would like to try out the new ultra low power driver on our board. Everything works fine with the full driver. However, we are facing a problem on VL53L1X_ULP_SensorInit() when using the ultra low po...

ALai.1 by Associate II
  • 2394 Views
  • 2 replies
  • 0 kudos