2022-12-06 8:38 AM
I was wondering if all the VL53L* sensors use the same VCSEL illumination source with the same average and peak power. I would think the the long-range sensors (VL53L1CB) and the sensors with wide FoVs of 63 degrees, would need a more powerful VCSEL.
2022-12-07 5:39 AM
There are not using the same VCSEL illumination source as it impacts the different features reached.
So ST is using a set of different VCSEL.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.