2022-11-29 7:53 PM
We have been using the full driver for VL53L1X and would like to try out the new ultra low power driver on our board. Everything works fine with the full driver.
However, we are facing a problem on VL53L1X_ULP_SensorInit() when using the ultra low power driver. It always return VL51L1X_ULP_ERROR_TIMEOUT as VL53L1X_ULP_CheckForDataReady() always return 0. We believe the I2C driver is working properly as it return 0x03 on reading VL53L1X_ULP_FIRMWARE__SYSTEM_STATUS on earlier state of the init routine.
2022-12-06 8:44 AM
Hello,
On ST side, we validated the code using ST boards. Are you using our boards or another one ?
2022-12-07 12:50 AM
We are using our board with STM32L072 and a VL53L1x. We have been using the full driver and everything works fine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.