Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X orientation and ROI

Dear,I want to implement a people counting algoritme using the VL53L1X ToF sensor. I want to build my own PCB for it. I found out that when the sensor is rotated by 90 degrees (gold filters in a row), the edges of a door are measured better then when...

SBann.1 by Associate II
  • 1333 Views
  • 1 replies
  • 0 kudos

Resolved! PerformRefSpadManagement doesn't work

This is the detailed log of the I2C communication between an ESP32 and a VL53L4CX[I][logger:242]: Log initialized [VV][esp32.preferences:070]: nvs_get_blob: key: 233825507, len: 4 [C][ota:469]: There have been 0 suspected unsuccessful boot attempts. ...

IHern.2 by Associate III
  • 4321 Views
  • 8 replies
  • 0 kudos

Unable to FW Flash on X-NUCLEO-6180A1

Hi, I am having issues getting my X-NUCLEO-6180A1 to work with the NUCLEO-F401RE. I have followed the instructions in the manual and the troubleshooting guide, although still cannot get things to work. I believe I need to flash FW manually. alth...

RHill.4 by Associate II
  • 4104 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L8CA footprint, initialization time and comparison

Hi,I have some questions about the latest ToF released VL53L8CA (only databrief released at the moment):Is the VL53L8CA footprint/pinout-compatible witth the VL53L5CX?Is the VL53L8CA on-board microcontroller RAM-based (like VL53L5CX)? If yes, what is...

MFabb.1 by Associate II
  • 3171 Views
  • 4 replies
  • 0 kudos